Hi Eva,
Per talked, we can follow up below discuss here:
Thank you!
Marc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Marc,
I closed your other post and will just respond here then.
Originally you mentioned the device was failing at about 300V, and now it is failing at 450V, is that correct? Did the customer change anything between these two trials?
It looks like the failure the customer is seeing is that the high side is powering down. I think this is because the high-side power supply is under the recommended operating conditions. This should typically be 5V, but at least 4.5V. Looks like the customer has it at 3.3V. If the power supply is inefficient, the amplifier’s offset error and drift could increase or other unexpected behavior.
Please let me know if this fixes the error!
Best regards,
Eva