Part Number: THS4631
a. Is there a protective diode built in between the input terminals of the THS4631?
b. If it is built in, can you tell me the current-voltage characteristic and the conditions under which it is used?
For example, as follows,
Vf = 710mV(typ.) @ If=1mA, Ta = 25℃