Part Number: OPA2182
Other Parts Discussed in Thread: OPA2350, OPA2187, OPA2189
hello we use the OP2182 as a buffer for the reference voltage

the amplifier is overheating to 85°C we check the power consumption it is 58mA, to be known that the component power tow reference circuit
for TX : 
For RX : 
We desolder the component while powering the output (pin 1 and 7) via a power supply to emulate its present we have 1,5mA output current consumption
we tryed to power the OPA2182 via external power supply (pin 8), we noticed that when the opa is powered at 6,8V it is consuming 3,5mA when it is powered at 6,9V it consumes 40mA, in both cases the output is 5V
I noticed that the ref on the component is : OP2182

please can you help us with the root cause to solve the issue
best regards
Ziad