Other Parts Discussed in Thread: LMH5401-SP
Suggest a Aerospace Grade equivalent of LTC6406IMS8E#PBF from TI
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Suggest a Aerospace Grade equivalent of LTC6406IMS8E#PBF from TI
Hi Shyam,
We have a few fully differential amplifiers that are space rated, I attached a link below that lists all of them. If your bandwidth requirement is in the 3GHz range, I would recommend the LMH5401-SP. If this is a part you are interested in I can forward this thread to the appropriate team to further assist you.
Fully differential amplifiers product selection | TI.com
Best Regards,
Ignacio
Hi,
My apologies
I have to correct my statement.
I am looking for Avionics Grade which must be suitable for Air Platforms, Not Space Platforms/Programs
Here in my case its DO-254 Compliance, which is widely followed for ASIC/FPGA/ICs.
Kindly educate me here, when your customers chose parts for Avionics grade do they use AEC Qualified parts for adapting reliability, or will be using special space qualifying ICs ?
Here i am aware that AEC is not a standard for Avionics / space, but people choose for better reliability i assume, so that they can qualify entire board for DO-254 screening.
Hello Shyam,
Does this mean you do not need the space qualification (-SP, -SEP) which would mean devices that qualify for QML Class B and Class V in accordance with MIL-PRF-38535, links for more information can be found here:
Or do you need a high reliability part (-EP) which would be in accordance with GEIA-STD-0002-1
Or automotive qualified which would be in accordance with AEC-Q100
TI provides documentation for functional safety that our customers can use in order to support DO-254 certification of their systems. For Functional Safety Compliant devices, this documentation includes FMEDA, FTA, etc, as can be seen below. Additional information can be found at Functional safety | TI.com
Thank you,
Sima
Your were right , i wish to follow the MIL-PRF-38535 standard
I wish to see the parts in Opamp/ADC/Regulators qualifying this standard.
Hi Shyam,
That standard will fall under space qualified devices. The best option for that case was the original space grade device I recommended.
Best Regards,
Ignacio