This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP7704-SP: 5962R1920601VXC - Tolerances on Drawing Question

Part Number: LMP7704-SP

Hello,

I'm currently working on a design with the part 5962R1920601VXC (or the LMP7704-SP).

From the datasheet, there are given dimensions of 0.43mm MAX (from the bottom of the part to the leads) and 25mm MAX (lead tip-to-lead tip).

Could your team provide the Minimum values for these dimensions?

If it helps, from the DLA Land & Maritime drawing, these dimensions would the the "A1" and "E3" dimensions.

Thanks!