Part Number: OPA2171
Other Parts Discussed in Thread: OPA2607, OPA2991, OPA2992, OPA2990
Hi team,
Customer use OPA2171 to sample the primary current in LLC topology.
They use to parallel LLC to extend the power, and OPA2171 is used to sample two primary current in the resonant tank.
When the output voltage is 650V and add full load at the output, OPA2171 have a certain possibility that output voltage can't match the input. Frequency is 122K.
But if they change to OPA2607, everything will be good. OPA2607 have less Offset.
Schematic:


Yellow: primary current 1 Green: Primary current 2 Blue and Purple: Output of OPA2171
OPA2607: Blue primary current, purple: OPA2607 output
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/14/OPA2607.jfif