Part Number: CIRCUIT060074
Other Parts Discussed in Thread: TLV1861
Hi BU team,
Hope you are doing well!
My customer is interested in using comparators to do OCP. Can you help design a current comparison circuit that meets my customer's requirements?
Here are the application requirements:
- Common voltage is 40V
- The sensor resistance is 10mR
- Trigger current is 3A and 6A
Here are some questions about CIRCUIT060074 from customers:
- What is the accuracy of current sensing?
- What is the response time from when the current reaches the trigger value to when the op amp outputs low?
- Is there an EVM?
Thanks in advance!