Hi team,
I'm planning to design a circuit having a TLV3605 with an FPGA to capture some analog signals. The analog signal is a randomly fluctuating signal fed to the non-inverting terminal of the comparator TLV3605 and a reference voltage is given at the inverting terminal of the comparator TLV3605. I'm wondering whether it's possible to use the 300MHz or lower clock signal from the FPGA to synchronise the comparator output using the latch functionality of the comparator? If not, is there any other solution to achieve this?
Here's the image of a similar setup I found in the datasheet. I was wondering if there's a way to synchronise this with FPGA using the Latch functionality at 300MHz or less. Feel free to purpose any other comparators or ICs that can do the job.