Part Number: OPA2330
Other Parts Discussed in Thread: OPA333, OPA350, OPA320
Hello,
I have a circuit where both channels of the OPA2330 (full part number OPA2330AIDGKT) are configured as a simple unity buffer. A 3.0V input on both channels comes from a precision reference (REF3430MDBVTEP). Each output drives VREFHI for 2 ADC banks on an MCU (TMS320F28377DGWT-EP). The issue is that the opamp outputs are 1.85V, not 3.0V as was expected. The output is not being loaded by any device other than the VREFHI input pins. The issue exists on both channels and across multiple circuit boards that were tested. We are unable to identify any issue with the implementation.
We are operating the ADC banks in 12-bit mode and, per the suggestion on the microcontroller datasheet, there are 1.0uF bypass capacitors near each of the VREFHI pins, totaling 2.0uF in total between the net and GND; however, these are not shown on the circuit snip below.
This circuit is implemented in a similar way on the LAUNCHLX evaluation board which featured a buffered and filtered precision reference voltage driving two ADC banks.
See circuit diagram:
Thank you for any insight.
Tom