Hi All,
I am designing the transimpedance amplifier circuit using OPA2846. There is an example for a two-stage amplifier in the data sheet.
The example is for 100k ohm transimpedance amplification. But my signal is very weak around 50nA.
So I need 8M ohm transimpedance gain. I design 200k ohm in the first stage and the second stage gain is 40.
Is the opamp suitable for this amplification? Will the opamp be a stable opamp for this application?
The circuit is as shown below.
Thanks,
Thomas