This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV2186: Similar part with shutdown

Part Number: TLV2186
Other Parts Discussed in Thread: OPA2734, OPA2334

Hi there,

Is there a part that someone can recommend with similar characteristics to the TLV2186 but also with a shutdown pin? I have some instabilities using this opamp in a composite opamp circuit (this opamp drives the input of another opamp) where the second opamp in the chain has an enable line and this causes some instabilities when enabling/disabling due to the TLV2186 going to its full output when the second opamp is disabled (ie the feedback is disabled). 

If there is no similar part you can recommend or is there any other workaround I can do do manage the TLV2186 output at zero volts when the second opamp is disabled (feedback is disabled). 

I know this is quite a tricky situation. Thanks in advance for any advice,

Steven