Good Morning.
I'm using INA310A3 for mesuring current between 50mA and 2A.
By measuring with a scope, the INA310A3 ouput voltage, I have a 7% error (264mV for a real current through the shunt of 120mA, checked with a serial amperemeter).
The 0,02ohm shunt has an accuracy of 0,5%.
Taking into account the 0,05% shunt accuracy into LTspice simulation, the output voltage error value is 1,1%, which seems to be more correct.
The schematic is the one above.
What may cause this 7% error ?
Thanks per advance.