This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP2012QML-SP: Common Mode Input Range (recommended max specification)

Expert 4545 points

Part Number: LMP2012QML-SP
Other Parts Discussed in Thread: LMP2012

Hi TI Amplifier Team,

Customer came across a weird behavior during the simulation, the common mode voltage cannot go above a certain voltage (on the positive side). There is no mention in the datasheet of a maximum working common mode voltage for its input, but some graph stops at 3.5V for a 5V supply.

Can TI elaborate on what is the maximum recommended (not abs max) common mode voltage of this part, relative to the supply voltage?

Thanks a lot in advance & BR,
KF