Hi,
Here is my scenario. I have 2 voltages (one coming out of the TI DAC1220, the other from a voltage reference chip for 2.5V). I want to make the 2 voltage source go into a +Sig and -Sig input of a device. The difference of the voltage can be in the uV range (as low as 4.7 uV difference).
Can I use this op amp to make it so that I have as little noise as possible (< 4.7uV between the 2 signals)? If so, how do i connect the 2 signals to the op-amp?
Thanks,
Paul