This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Experts,
This board will be used for designing a probe for measuring switching currents of a high-speed SOC.
The input voltage range is expected as 250uV to 7.5mV.
OPA891 and OPA892 have offset nulling pins. The offset voltage drift is 1uV/C.
Two OPA891 will be used as unity gain buffer (stage 1) for P and N differential input. OPA892 will be used as a differential to single ended amplifier with a gain of 20 (stage 2). Another noninverting amplifier of OPA892 with gain of 20 (Stage 3).
Is OPA891 and OPA892 suitable for my application considering it has input offset voltage null pin?
Following parameters of OPA892 are important for this choice:
1. Output current drive of 200mA.
2. High slew rate.
3. Gain BW product
4.Flat closed loop voltage gain.
thanks, Abhijit
Hi Abhijit,
I was wondering if you could share some details on the specs you require. For the BW and slew rate is there a goal or minimum required in the design. The devices you listed could very well work in this application and the benefit of the null pins help reduce error in your application.
Best Regards,
Ignacio
Hi Ignacio,
Specifications are below:
Question:
thanks, Abhijit
Hi Abhijit,
Could you also share the supplies you are working with. One consideration with the OPA892 is the minimum supply requirement of 9V. As for your questions, yes, the OPA892 will support that output swing in a gain of 14V/V. The gain of a device wouldn't affect the output swing of the device, other factors such as output current and supply values would affect the output swing. To answer your second question, the null pin feature was meant to reduce the offset beyond the typical Vos spec.
Best Regards,
Ignacio
Hi Ignacio,
Will the offset voltage of OPA2892 will be matched in the same direction or it will cancel out each other? There is no null pin for OPA2892.
thanks, Abhijit
The offsets of the two OPA2892 amplifiers are random, i.e., the might go in the same or in different directions, and are likely to have different values.