Part Number: THS4522
Other Parts Discussed in Thread: THS4521, THS4551
Hi,
I am trying to simulate a new design using LTSpice.
I downloaded the Spice model as a zip (sbom343e.zip) file from the TI website.
I am using ths4521.lib from the zip file.
Vdd = 3.3V
Leaving VOCM pin unconnected, the output voltage sits at 2.49V but shoudl sit a 1.65V as per Datasheet.
Connecting VOCM causes the simulation to not solve.
There is also no amplification showing when I apply a signal to the inputs and gain set to 47 (using RF= 470k and RG=10k)
Is there a better working model for this part perhaps or a workaround?ths4521_a.lib