Part Number: ISO224
Other Parts Discussed in Thread: AMC3330
Hi,
I am trying to build a circuit in which an incoming analog control signal (0-10V), with a precision of 16 bits, is galvanically isolated and then output with the same precision, ideally identical. I was recommended the ISO224 for this purpose, but I am not sure if it is the right component. Ultimately, the circuit should be compact enough to be directly integrated into the control cable, requiring minimal space and additional wiring.
Basically i get a analogous 0-10V signal from a PLC and "only" have to relay the signal after galvanically isolating it from the input side. ideally i would create a small pcb that can be placed in-line with the existing wirering...
Any ideas?