Hi Team
I am looking for a analog isolator.
Input : 5V AC (Sinewave)
Output : 5V AC (Sinewave)
Please suggest.
Best Regards
Emil Jose
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
5 V RMS corresponds to about 7.07 V. The only device with this input voltage range is the ISO224, but you could use another one if you divide down the signal.
The ISO224's output does not go above 4 V; you need to amplify the output.