Part Number: INA180
Other Parts Discussed in Thread: TPS62933
Hi,
I would like to measure the DCDC buck Iout. The DCDC chip TPS62933 is operating correctly: stable Vout=12V, clean PWM signal, temperature is OK. I'm using E-load to draw stable 1A, 2A and 3A output current from DCDC.
As suggested in another thread, I should place the current sensing resistor after output capacitors. However, the current sensor output is still a sine wave, also wrong amplitute.
Please help, thank you very much.

500kHz PWM SW signal:

When Iout = 1A, current snesor output is:

When Iout = 2A, current snesor output is:

When Iout = 3A, current snesor output is: