This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH6553: Simulation

Part Number: LMH6553

Hi, 

I am trying to simulate a circuit with the LMH6553, but the simulation gives an error with the following message:


** Creating circuit file "Trans.cir"
** WARNING: THIS AUTOMATICALLY GENERATED FILE MAY BE OVERWRITTEN BY SUBSEQUENT SIMULATIONS

*Libraries:
* Profile Libraries :
* Local Libraries :
* From [PSPICE NETLIST] section of C:\cds_spb_home\cdssetup\OrCAD_PSpiceTIPSpice_Install\23.1.0\PSpice.ini file:
.lib "nom_pspti.lib"
.lib "nom.lib"

*Analysis directives:
.TRAN 0 5u 0 1n
.OPTIONS ADVCONV
.OPTIONS FILEMODELSEARCH
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*))
.INC "..\SCHEMATIC1.net"

**** INCLUDING SCHEMATIC1.net ****
* source LMH6553 WITH ADC
R_R9 OUT+MATCHED OUT-MATCHED 100 TC=0,0
R_R2 IN- N02889 348 TC=0,0
C_C2 N02519 OUT- 1p TC=0,0
V_V3 N02823 0 0.75Vdc
R_R3 IN+ N02519 348 TC=0,0
R_R8 OUT- OUT-MATCHED 50 TC=0,0
R_R6 N02519 OUT- 348 TC=0,0
V_V7 IN- 0 AC -0.5
+SIN 0 -0.5 60meg 0 0 0
R_R7 OUT+ OUT+MATCHED 50 TC=0,0
V_V6 IN+ 0 AC 0.5
+SIN 0 0.5 60meg 0 0 0
R_R5 0 IN- 59 TC=0,0
R_R4 IN+ 0 59 TC=0,0
V_V2 N02609 0 -5Vdc
R_R1 N02889 OUT+ 348 TC=0,0
C_C1 N02889 OUT+ 1p TC=0,0
V_V1 N03422 0 5Vdc
V_V8 N03533 0 1.2Vdc
X_U3 N03422 N02609 N02519 N02889 OUT+ OUT- N02823 N03533 LMH6553

**** RESUMING Trans.cir ****
.END
X_U3.q9 X_U3.a140 N02823 X_U3.a149 0 X_U3.NPNXTR
X_U3.q1 X_U3.a176 X_U3.a134 X_U3.a252 0 X_U3.NPNXTR
X_U3.q10 X_U3.a146 X_U3.a148 X_U3.a174 0 X_U3.NPNXTR
X_U3.q11 X_U3.a149 X_U3.a134 X_U3.a222 0 X_U3.NPNXTR
X_U3.q3 X_U3.a119 X_U3.a111 X_U3.a154 0 X_U3.PNPXTR
X_U3.q5 X_U3.a111 X_U3.a111 X_U3.a157 0 X_U3.PNPXTR
X_U3.q4 X_U3.a199 X_U3.a111 X_U3.a160 0 X_U3.PNPXTR
X_U3.v2 X_U3.a241 X_U3.a174 0
X_U3.v1 X_U3.a202 X_U3.a176 0
X_U3.i9 X_U3.a0100 X_U3.a0198 2.5e-6
X_U3.i5 N03422 X_U3.a148 12e-6
X_U3.i0 N03422 X_U3.a108 7e-3
X_U3.f2 0 X_U3.a203 X_U3.v2 1.0
X_U3.f3 0 X_U3.a205 X_U3.v2 1.0
X_U3.f1 0 X_U3.a205 X_U3.v1 -2.0
X_U3.f0 0 X_U3.a203 X_U3.v1 2.0
X_U3.rtm 0 X_U3.a205 128e3
X_U3.r29 X_U3.a222 N02609 250
X_U3.r30 X_U3.a224 N02609 250
X_U3.r31 N03422 X_U3.a113 250
X_U3.rtp X_U3.a203 0 128e3
X_U3.r32 N03422 X_U3.a115 250
X_U3.r20 N03422 X_U3.a157 250
X_U3.r15 X_U3.a0113 X_U3.a148 2.5e3
X_U3.r22 N03422 X_U3.a160 175
X_U3.r16 X_U3.a148 X_U3.a0117 2.5e3
X_U3.r33 X_U3.a149 X_U3.a241 200
X_U3.rtc X_U3.a108 N02609 14.3 tc1
-------------------------------$
ERROR(ORPSIM-16015): Unknown parameter.

I suspect that the error is due to the missing parameter tc1 and tc2 any help?