Part Number: INA214-Q1
Other Parts Discussed in Thread: INA214,
Dear TI
I have question
Rshunt = 0.02 ohm
IN+ = 7.5V
V+ = 3.3V
Question
1) INA214 gain is 100.
If Consumption current (I shunt) is 0.1A, OUT pin voltage is 0.2V? Is it right?
If V+ voltage is 3.3V, is there no problem up to 1.65A current? ( Out voltage = 3.3V)
2) If Consumption current (I shunt) is 0mA, How much is the IC consumption current?

Thanks