This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA214-Q1: Question about INA214

Part Number: INA214-Q1
Other Parts Discussed in Thread: INA214,

Dear TI 

I have question

 Rshunt = 0.02 ohm

IN+ = 7.5V

V+ = 3.3V

Question 

 1) INA214 gain is 100. 

   If Consumption current (I shunt) is 0.1A, OUT pin voltage is 0.2V? Is it right? 

   If V+ voltage is 3.3V, is there no problem up to 1.65A current? ( Out voltage = 3.3V)

2) If Consumption current (I shunt) is 0mA,  How much is the IC consumption current?

   

Thanks