This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA219: INA219AIDCN Failure

Part Number: INA219

We encountered a high fallout in production due to this component.  The power register consistently shows a zero reading, with an observed occurrence of 28% across 100 tests. Notably, these failures are not consecutive. The oscilloscope is configured to trigger on I2C bus activities, and the power monitor test is manually initiated. The test is halted upon detecting the failure waveform.

Need your help to check whether there are any issues reported for Texas Instruments MPN# INA219AIDCN worldwide.  Are there any datasheets changes or PCN about the changes for this INA219AIDCN?  

The date code impacted components are D2312, D2343, D2344, D2348.