Part Number: LM7322
I'm using the LM7322QMA/NOPB operation amplifier in a project, The opamp is powered with 24 V single supply, I measure 0.5 mA to the inverting and non inverting input pins. Based on the LM732x datasheet indication the input bias current has to be less than 0.002 mA. I tried the LM7322MAX/NOPB but the measured value is the same.
How is it possible?
TI field application engineer, could you explain me why?
Many thanks
Regards