This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV4062: TLV4062 parallel and as Time Multiplexing

Part Number: TLV4062
Other Parts Discussed in Thread: TLV9062

Tool/software:

Hi team,

Is it possible to create a parallel TIA AC-coupled contract phase amplification circuit as shown in the attachment with a TLV9062 or 9064? As shown below, the frequency 1 to 3KHz signal can be detected and the current source can be used instead of the PD. Is it possible to design time-to-time multiplexing between U1 and U2? Could you help to provide waveforms through experiments or simulations?