This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA290: Inquiry about device usage range

Guru 12795 points

Part Number: INA290

Tool/software:

Hello,

In the INA290 Datasheet, the Vcm range is specified as Vs(V) ~ 120(V) as shown below.

If the INA290's Vs is supplied at 3.3V, then both +12V and +3.3V are within the current sense range, and if the INA290's Vs is supplied at 15V, then both +12V and +3.3V are not within the current sense range?

Thank you.

JH