Hello all,
I'm working with a customer that is using the INA326 instrumentation amplifier and is simulating in TI-TINA. After working out the calculations in the datasheet, my customer tries those values in TINA and they do not match the expected result.
I'd appreciate if someone could take a look to see if I missed anything obvious.
According to the datasheet and Mathcad, these resistor values should give a gain of unity and an offset of 1.5V. However, with an input of -1.5V the output is 412.66mV (when it should be 0V). An input of +1.5V will yield only 2.57V (when it should give 3V). What is wrong with this picture?
Thanks!
-Richard

.