This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA250: current flow and output mismatch

Part Number: INA250
Other Parts Discussed in Thread: DRV103,

Tool/software:

Hello,

I am using INA250A4 and connected to +vs and the one side of the  valve, other side of the valve is connected to pin no 5 of DRV103. From INA250A4 I am getting 550mV out which means 275mA of current flowing though the valve according to the datasheet of INA250A4. but when I put multimeter in series( between IN- and the  valve) to measure the current it only shows 127mA, if I connect the multimeter on the other side(valve and pin 5 of DRv103), I get 127mA. What might be the problem, is this something obvious, or my connection is not right.?