This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA238: I2C communication failed / no ACK

Part Number: INA238
Other Parts Discussed in Thread: INA226

Tool/software:

Hi,
among 3 other I2C devices, we have an INA238 on our PCB.
The I2C communication with INA238 (0x40@7bit) failed (no ACK), while the other I2C devices on the bus send an acknowledge.
We have no address conflict, the I2C signals at SDA and SCL (edges, start, stop conditions ...) are looking good, also supply 3.3V is OK.
Fscl~ 350kHz (no high speed mode)


Does anyone has an idea what went wrong?
Is there a special command routine needed?

Thanks in advance
Thomas Sagcob
Siemens Electronic Design Automation