Part Number: RCV420
Tool/software:
Hi everyone,
I'm thinking of using the RCV420 for my application. It will be used to convert the signal of a RTD measuring converter(4mA to 20mA) to a 0V to 5V or 0V to 3,3V. However when reading the theory of operation in the DS I noticed 16mA being used for the calculations. Can someone explain the reason for this?
Thanks in advance.
Kind regards,
Kavita