Part Number: INA226
Tool/software:
Hello,
In the datasheet, the maximum quiescent current is specified as 420uA. However, in figure 17, the current is shown to exceed 420uA when the I2C frequency increases past 1MHz.
Was the 420uA maximum determined using 400kHz I2C speed? Do you have a spec for the maximum quiescent current if the device is operating at maximum I2C frequency and maximum temperature?
Best regards,
Zach Kimble