Other Parts Discussed in Thread: OPA2156, OPA2277, OPA211
Tool/software:
Hi All,
I'm trying to design the input stage driver for the ADS8568, from the datasheet here is the input stage

Using the analog engineers calculator I got the following values:

I selected the OPA2156 as the driver and have a 5V fixed input for now (first trying to get the input settling correct before any signal conditioning circuitry is added).
Running the OPA2156 in open loop I have the output as:

The acquisition time is set to 280ns and the sampling rate is 400k.
For the life of me using the recommended values I cant get it to settle within 1/2 LSB which is ((10V/65535)/2) = ~76uV
Here is one of the simulations I ran:

The GBW of the amplifier is within spec and I'm not sure why the amplitude does not settle sufficiently.
Any help will be appreciated.
Thanks in advance