Tool/software:
Hi TI experts,
Now We want to use LMH6518 to driver high speed ADC. Vcm from ADC is 0.9V.
Question1: What is the range of Vcm input about LMH6518(indulding min/typ/max)
Question2: What about setting up the Vcm pin input to 0.9V, what is the impact on output and performance?
I see that recommended common mode output is from 0.95V to 1.45V as below: