Tool/software:
Good day, colleagues,
I have a question regarding LMP7716QMME/NOPB,
The max. temperature according to the specifications is 150°C.
Customer is asking to estimate the risk over lifetime by having higher maximum temperatures.
There are 2 cases we should look at:
- 100h@151°C & 400h@136°C
- 100h@152°C & 400h@137°C
Can you please give a fit rate for the risk using the part at that higher temperatures over the given number of hours for a lifetime estimation?
Thank you,
Daria