Other Parts Discussed in Thread: OPA891, OPA365, THS4531A, THS4521, OPA836
Tool/software:
Presently I have a system working fine, except it is picking some noise from a neighboring system.

The noise is picked up by the ribbon Cable, Therefore i was thinking of making the single ended signal to differential so that the noise picked by the cable is same and hence gets cancelled out.
I do not want to make any changes on my present ADC board (except of adding a Differential to Single ended conversion small board in front side)
New scheme looks like below

Single Ended signal specs
Range: .3V to 3.5V
Clock: Maximum 4MHz
I would like to get the same signal at the ADC after the differential to single ended conversion. Can you please suggest suitable IC for the New Board (differential to single ended conversion) ?
ADC is samples at maximum 16 MHz.