Tool/software:
Hi everyone,
I'm working with the OPA836 and I need to design a peak detector. I'm using the simplest circuit to simulate it, as shown in the following figures.
Some characteristics of the OPA836 for the peak detection circuit:
- Slew rate = 560V/μs
- Voffset = ∓65μV
The difference between the figures is just the input voltage offset (since I'm working with a single power supply).
I want to detect signals with a rise time of 50ns, so I used a 5MHz sinusoid to obtain this rise time in 1/4 cycle. At this frequency, Xc1 = 21k.
What's wrong with these circuits? What am I forgetting? This is the simplest peak detector circuit, but I can't get it to work based on the OPA836.