Other Parts Discussed in Thread: INA219
Hello All,
I'd like a little help and insight from folks regarding the INA219. I have a customer using the INA219 to measure a current --
The current will vary from 0 to 2.5A he needs a resolution of 50 mA steps. However, when taking a reading the INA219 is off by 125% or more. Even at 0A, the device still reads 28 mA of current.
Anyone have any ideas why this would occur? Of course all bets are off with ESD and the like, but has the factory seen this behavior?
Thanks!
-Richard