Part Number: INA331
Other Parts Discussed in Thread: OPA336, INA351, LM7705, OPA333
Tool/software:
For instrumentation amplifier, INA331, this is being used as differential amplifier with R1 = 100K digipot and R2 = 100K. From DS, this indicates that VREF requires to be driven with low impedance input. To acheive low impedance for VREF, this has been implemented as follows:
Digipot, L connected to 0V.
Digipot, W connected to input of buffer, OPA336, with output connected to VREF
Digipot, W connected to RG input on INA331 along with one side of R2, 100K. Other side of R2 connected to Vout.
Please advise if above configuration outlined allows:
Varition of Gain as digipot is used as variable resistor in expression, G = 5 + (5R2/R1)
VREF is driven from low impedance, OPA336
If you are able to provide an update ASAP please ?
Thanks