Tool/software:
I am looking at the datasheet of OPA2145. I am wondering about the maximum output current of this OpAmp. The datasheet says "Short-circuit current" +/-20 mA. Is this the maximum current at OpAmp output ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
I am looking at the datasheet of OPA2145. I am wondering about the maximum output current of this OpAmp. The datasheet says "Short-circuit current" +/-20 mA. Is this the maximum current at OpAmp output ?
How we can relate the maximum continuous output current to the short-circuit current ? Let's suppose an OpAmp is driving a voltage. What maximum current we can get. I notice that some data sheets only describe output current while some other only have short-circuit currents.
Hi John,
The devices are designed to withstand the short-circuit current as the maximum. Generally, if you are driving anything low impedance (i.e. a voltage source), the device will go into current limit. The maximum "continuous output current" is the current limit value.
This assumes the device does not go into thermal shutdown- if you load the output with a high current, the resulting power dissipation on the die can be high, and the device may go into thermal dissipation.
It may help to discuss this with a circuit in mind - do you have a specific circuit that will help narrow this down?
Regards,
Mike
There is no specific relationship between these values (except that the short-circuit current always is larger). The short-circuit current is measured when the output voltage drops to zero. The output current is specified for some other output voltage; the datasheet usually picks some voltage or current that it thinks is reasonable for this device.