Other Parts Discussed in Thread: XTR111, XTR117, XTR115
Tool/software:
Hello,
I am tying to use XTR116 for my 4-20mA transmitter project.
In this project, the sensor is 5-V sensor (together with a microcontroller) and they both draw about 300 mA.
I am planning to use XTR116, but the on-chip 5V regulator cannot supply such high current.
In addition, I would like to supply the whole system (i.e., sensor + microcontroller + 4-20mA transmitter) using only from the 2-wire 4-20mA current loop, without adding any extra DC supply for the sensor.
How could I realize this system ?
I have done some research, but it seems that there is no exact solution ...
Best regards and thank you very much,