Part Number: TLV3605
Other Parts Discussed in Thread: TLV3604
Tool/software:
What is the preferred method for implementing adjustable internal hysteresis with the TLV3605; using a pot (e.g. AD5235) or an adjustable current sink (DAC and BJT ) on the LE-bar/HYS pin? There are two things that I'm probing with this question; 1) Should extra capacitance on the LE-bar/HYS pin be minimized and 2) would a current sink give a more temperature stable Hysteresis level by avoiding the temperature variation of the DC level of the LE-bar/HYS pin?