Part Number: LM5158
Tool/software:
WEBENCH selects a transformer VP2-0066R from Eaton, but calculates the wrong series resistances.
I entered the following data to WEBENCH:
VinMin = 16.0V
VinMax = 32.0V
Vout = 4.0V
Iout = 1.5A
Device = LM5158RTER
Topology = Flyback
The VP2 transformers have 6 coils, which aer connected to result in:
Lp= 12.8 µH, Rp= 90.0 mOhm, Leakage_L= 166.0 nH, Ns1toNp= 500.0 m, Rs1= 90.0 mOhms, Ns2toNp= 1.0, Rs2= 180.0 mOhms
As Lp is acheived by connecting two coils in series Rp should be 180mOhm and Rs2 should be 90 mOhm to my understanding.
Did I undertssna dsomething wrong, or is there a bug in WEBENCH?