Other Parts Discussed in Thread: AMC1300
Tool/software:
Greetings,
I am using AMC 1350 and AMC1300 for sensing current and voltages and I am reading more than max rated offset errors in multiple instances. One of AMC1350 has an offset of 10mV DC at the inputs when resistor divider is shorted. Reading voltage across a resistor of 1M ohm with 10M ohm in series. The error is generally over the max rated value when tested on multiple AMC1350s. I have to short the differential input pins, bypassing resistor network to make it 0 and read 0mV on the other side.
The VCC is maintained at approximately 5.3V on both sides, with ripples under 2mV. I am measuring AC and DC voltages around 10V and trying to not burden the circuit I am sensing and hence upped my resistor bridge from 2.27MOhm to 11MOhm. U9 is my AMC1350 in the pic below.
My issues are same as this post: AMC3311: Offset problems due to interference and bad layout? - Amplifiers forum - Amplifiers - TI E2E support forums
I would greatly appreciate any insights or suggestions you might have to address these discrepancies. Your expertise is invaluable to us, and any guidance on mitigating these offset errors would be highly beneficial.