Part Number: INA241A-Q1
Other Parts Discussed in Thread: INA190, INA186, INA237, INA239, INA228, INA229, INA226
Tool/software:
We need to monitor the current through a Shunt resistance of 40mOhm.
For the diagnostic purpose, we are planning to keep 1K ohm resistor in series between the IN+ & IN- pins and the shunt resistor.
So now the questions are,
1. Is it allowed to have 1K ohm resistance in front of IN+ & IN- pins of INA241A-Q1 device?
2. What is the functional impact of having high input resistance in front of IN+ & IN- pins of INA241A-Q1 device?
3. Is there any formula or simulation is available to estimate the impact of INA241A-Q1 device due to this configuration?