Other Parts Discussed in Thread: TL431, TLV9061
Tool/software:
I have a sensor with an output range of 50mV to 500mV relative to ground. I need to convert this signal to a 0-5V range (or another suitable range) for measurement with a 10-bit ADC. I'm considering using the INA350 current sense amplifier and have installed the Analog Engineer's Tool.
My current setup:
- Vs+ = 5V
- Vs- = 0V
- Gain = 10
- Vref = 0V
Questions:
- Is this configuration appropriate for my application?
- How should I handle the common-mode voltage (Vcm) in this circuit, given that my sensor output is ground-referenced?
- Can you provide a basic circuit diagram for connecting the INA350 in this application?
- Are there any additional considerations or components I should include for optimal performance?
- Can I use the TL431 for providing a reference voltage in this circuit? If so, how should it be implemented?
I'm not an analog engineer, so I'd appreciate any guidance on implementing this circuit correctly.