Other Parts Discussed in Thread: REF200
Hi,
I am in the process of a designing a project and I need a floating adjustable current source. The REF200 looks like a promising little chip and in both the datasheet and application notes (SBOA046) for it there are circuits that do almost exactly what I want to do. The circuit I'm specifically talking about is Figure 10e in the datasheet and Figure 16 in the application notes. The circuit is specified as a Floating Current Source for outputs greater than 100uA.
For my project, I need a floating adjustable current source just like this one, except I need outputs as low as 10uA.
If anyone has insight or previous experience with this chip that could help me adjust this circuit to allow current outputs down to 10uA it would be greatly appreciated.
Thanks!
Kyle