Other Parts Discussed in Thread: LMV1012, , OPA375, LP2982
Tool/software:
Hi, Ti.

Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi, Ti.

Thank you.
Hello Yunsik,
LMV1012 (not my group) has a voltage gain spec. Connecting it to an op amp inverting input (a virtual short) with a capacitor will AC short out the LMV1012 and the op amp amplifies the shorted current into an output voltage. I expect this is not what you wanted and not what the LMV1012 expected.
Try adding a resistor in series with TC4. 1k ohms for 40dB gain in TLV9361, but lower cutoff goes to 70Hz. AC load is now 1k ||2.2k =687 ohms not 2.2k , so LMV1012 gain may drop. So consider increasing R1, so new resistor can be larger too.
Hi Mr.Ron,
The schematic below is from a circuit I designed previously that operates with a 3.7V battery.
In that circuit, it worked properly even without a resistor at the inverting input of the op amp.
I'm curious about what's different in the above circuit that requires an additional resistor.

Thank you
Yunsik,
For the op amp , I don't see any meaningful change. I transferred this post to the engineer supporting LMV1012. He should know if this affect the LMV1012 or not.
Hi Yunsik,
It seems to me that the circuit is pretty much the same, you just replaced OPA375 with TLV9361 and increased the power supply range. However, the passive components associated with the op amp are the same, thus the same gain should be expected. Correct?
If you compare the signal output from LMV1012 between the two circuits, is there any difference?
Perhaps OPA375 tolerates the lack of input series resistor while TLV9361 does not.
Best regards,
-Ivan Salazar
Applications Engineer
Hi Ivan,
I confirmed that the virtual short of the TLV9361 is not functioning properly.
The op amp inverting input should show 3.7V, but it actually showed about 1V, and this was the same even with a series resistor added to TC4.
The LMV1012 is working properly, and it amplifies the signal by 30 dB.
Best Regards.
Hi Ron,
Below are the waveform photos from each pin.
I applied an AC 1mV to the input of the LMV1012.
The photos show the minimum and maximum values of the waveform.
Looking at the non-inverting input of the TLV9361, it is oscillating at 7.4 Vpp, which seems to be the problem.
Ground pin was 0V and power supply pin was 7.37V.
Non-inverting input pin

inverting input pin

output pin

Best regards.
Yunsik,
So odd to see huge oscillation on Non-inverting input, which is pin 1 in the schematics. I see nothing on this pin that can output such a signal.
If the DBV package was used with board setup for DCK pinout, that could make such a signal.

Upon checking, I realized that the board designed for the DCK pinout was using the DBV package.
The issue has been resolved.
Thank you.
Best regards.