This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA216: An Error in the graph of product data sheet

Part Number: INA216


Tool/software:

I saw the following graph (Figure 13) in the INA216 data sheet and thought it was wrong.

For INA216 there is Vcm = V+, Output Voltage = Vsense*G, and the figure shows that Vsense = 100mV.

In the red box area of the figure below, when Vcm=2V, the Output Voltage should be equal to 100mV * G, but not 0V.