Other Parts Discussed in Thread: OPA197
Tool/software:
Hello TI,
I have a query regarding OPA197-Q1 output pin sink current during unpowered condition of the device. I could not find this information from the datasheet, however from the figure 7-12 in the datasheet, i undertsand that there are clamping diodes available on the output for ESD protection. But in my application i might encounter some transient current of 40mA for 100us flowing into the output pin when the device is unpowered. Could you please let me know if this condition is acceptable for the device or the maximum allowable current that the output pin can sink/withstand for 100us without causing permanent damage to the device when it is not powered.

Best Regards,
Manoj.