Part Number: TL331
Tool/software:
Need to know the maximum junction temp for below part:-
| TL331KDBVR |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Gauri,
As Clemens showed, maximum junction temperature is 150°C.
Do note that this is the maximum temperature that will not cause damage, but the specified operation maximum temperature is 105°C. So the temperature should not exceed 105°C for proper operation.